E-Series failed to set constant bitrate

Description Seems to happen with context stream on e-series encoder. The range on constant bitrate mode could be set to invalid ragne of 32-1024 instead of 32-8192. So with bitrate set to something like 2048 would the bitrate out of range error and failed to set. Also in this case, the stream setting would also… Continue reading E-Series failed to set constant bitrate