Web service cannot connect to multiple servers at the same address

Description If web service with more than one server at the same address, but different ports, those servers are not treated independently. When accessing these servers through the web service, only the first will handle requests. <br> Version Introduced 7.5.32 <br> Platform All <br> Steps to reproduce Configure two servers at the same IP with… Continue reading Web service cannot connect to multiple servers at the same address