Affected platforms exacqVision Server 7.2.0 <br> Symptom Once successfully connected to an Entrapass server, changes to any connection parameters (IP address, port, username, password) are ignored. The connection will continue to attempt connection using the prior settings. <br> Workaround Dsiable the existing connection and create a new connection with new parameters. <br> Resolution Update to… Continue reading Changes made to Entrapass connection parameters in exacqVision client are ignored