Onvif mis-handle partial socket receive and could cause delay in connection

Description This bug caused the Onvif configuration failed to handle a complete soap message when they are partially send. The end result is that there would be a long delay before the camera would be “connected” <br> Version Introduced r34959 (dev build 5_1_9_34964) <br> Platform All <br> Steps to reproduce Use the Hitachi DI-CB320G(F8-48-97-9E-76-9E 10.16.11.47:8080 root/admin)… Continue reading Onvif mis-handle partial socket receive and could cause delay in connection