Objective Installing 32-bit Enterprise Manager on a 64-bit Ubuntu 14.04 or 16.04 Linux computer, complete the following steps: <br> Instructions Configuring a new system. <br> Setup multiarch <br> Remote Setup Ensure that X Windows can be forwarded to anyone using Putty or SSH (install gedit).Use Filezilla to transfer the debian installer to the instance.Connect using… Continue reading Installing 32-bit Enterprise Manager (EM) on 64-bit 14.04 or 16.04 Ubuntu Linux System