Description Affected platforms: Linux, Ubuntu 32-bit with PAE-configuration (systems with more than 4GB of RAM).Affected configuration: 1 DVR + n S-Series, where s-series are all used for Extended Storage and are being connected to the single DVR. <br> Symptoms A DVR system watchdogs while configuring many extended storage (iscsi) volumes. <br> Troubleshooting This is happening… Continue reading System watchdogs when configuring Extended Storage
Tag: Configuring
Configuring DS6716HQHI Encoder Streams
The following steps are intended for manually setting the certificate and key path for exacqVision Web Service versions 8.4 and higher. <br> Symptom When connected to a Hikvision DS-6716HQHI encoder, user sees seemingly random drops of video streams for a second or two. <br> Problem When this device detects motion, the encoder switches from the… Continue reading Configuring DS6716HQHI Encoder Streams