Installing 32-bit Enterprise System Manager (ESM) on 64-bit Ubuntu Linux System

To install ESM on a 64bit Ubuntu 12.04 Linux computer, complete the following steps: Configuring a New System Set up a 64-bit Ubuntu 12.04 image.Install ia32-libs and postgresql.Use a remote database engine (or install Mysql/Postgresgl locally) to create a database. Remote Setup Ensure that X Windows can be forwarded to anyone using Putty or SSH (install gedit).Use Filezilla to… Continue reading Installing 32-bit Enterprise System Manager (ESM) on 64-bit Ubuntu Linux System