Description Cloudvue Mobile v24.12 or higher is only supported on devices running Android Version 11 or higher. Product Solution Users running Android 10 or lower should update to Android 11 or higher.
Tag: Cloudvue Mode
Connecting an Analog Microphone to a Cloudvue C2C Camera
Cloudvue’s cloud-based recording solution provides the ability to record and playback audio. Many models of Illustra IQ cameras configured for Camera to Cloud (C2C) recording with Cloudvue’s services provide audio capabilities. Check your specific Illustra IQ camera model to determine audio support. Considering audio quality, refer to manufacturer recommendations and guidelines on microphone selection and… Continue reading Connecting an Analog Microphone to a Cloudvue C2C Camera
KT-1 Controller Firmware v3.09.xx Required For Cloudvue Mode
Description In addition to requiring a network with internet access the Kantech KT-1 controller must be running firmware v3.09.xx in order to run in Cloudvue Mode. Solution To determine the current firmware version, access the KT-1 controller from a web browser. Type https:// and the IPv4 address of the KT-1 or if using the MAC… Continue reading KT-1 Controller Firmware v3.09.xx Required For Cloudvue Mode
KT-1 Cloudvue Mode
Follow the process for preparing the Kantech KT-1 controller for Cloudvue mode as well as connecting it to a Cloudvue account.