Description When a camera is added to a Cloudvue Gateway it is assigned to that specific Cloudvue Gateway in our cloud database. Attempts to add the camera to a different Cloudvue Gateway will fail with a message indicating that the camera “Already Exists”. Here are the appropriate steps to follow in the event a camera… Continue reading Moving Cameras Between Cloudvue Gateways
Tag: Cloudvue Gateway
Cloudvue NVR Recorder Debugging
Description At times it can be useful to get nvr-recorder debug level output to troubleshoot recording issue on a Cloudvue Gateway. This can be achieved using the smv-record debug engine. Product Solution The basic steps are: Example Tech Tip: Support Diagnostics also captures this information in the Smartvue-smv-record.log section.
Axis P3353 Cameras Not Recording on a Cloudvue Gateway
Title Axis P3353 Cameras Not Recording on a Cloudvue Gateway Description It has been observed that while live images are visible the Axis P3353 is not recording. Product Steps to Reproduce Expected Results Actual Results Solution
“Camera Save Failed” Message When Adding Camera to Cloudvue Gateway
*** INTERNAL USE *** Description Getting a “Camera Save Failed” message when attempting to add a camera to a Cloudvue Gateway. Product Steps to Reproduce Expected Results Actual Results Solution
Installing storcli on a Cloudvue Gateway
Description In order to interact with the RAID controller on a Cloudvue Gateway you must first install storcli. Products Steps Verification Confirm RAID Controller Present Use lshw to determine if a RAID Controller is present. If no results are returned then there is no RAID controller detected, thus no reason to proceed. sudo lshw |… Continue reading Installing storcli on a Cloudvue Gateway
Correcting Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif
Description Prior to the release of Cloudvue version 23.9 the error message “”Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif’” could appear when trying to add cameras to a Cloudvue Gateway. This will be fixed with the release of 23.9.x. Products Steps to Reproduce Add a new camera either by scanning or by IP. Expected Results Camera adds… Continue reading Correcting Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif
Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif
Description Prior to the release of Cloudvue version 23.9 the error message “”Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif’” could appear when trying to add cameras to a Cloudvue Gateway. This will be fixed with the release of 23.9. Products Steps to Reproduce Add a new camera either by scanning or by IP. Expected Results Camera adds… Continue reading Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif
Manually Updating Smartvue Software on a Cloudvue Gateway
Description At times it may be advantageous to manually apply production versions of Smartvue on a Cloudvue Gateway. Here are the instructions for obtaining, transferring, deploying, and verifying that software. Product Solution Example
Cloudvue Gateway Camera Integrations
Description Traditionally Cloudvue has focused on individual API integrations for cameras connecting to the Cloudvue Gateway. However, there are just too many camera manufactures to integrate with each. So, except for Illustra and Axis we rely on integrating with ONVIF Profile-S compliant cameras. Customers that would like a specific API camera integration should submit their… Continue reading Cloudvue Gateway Camera Integrations