Streams not closed when recording is disabled

Description With Dahua/Illustra Essentials, video continuous to stream when the recording for the stream is disabled in the ip camera recording page. Most likely this does not affect user but it affects traffic on the network. <br> Version Introduced r71495 (6.8.x RC) <br> Platform All <br> Steps to reproduce disable stream recording in the “Recording” tab of the… Continue reading Streams not closed when recording is disabled