Description exacqVision Client 7.8 introduced an issue when changing the time zone on a client running local to the server. The time sent to the server would be off by an hour or two. The workaround is to change the time zone, apply changes, then change the time and apply changes. <br> Tested Version <br>… Continue reading Issue when changing the time zone on a client running local to the server