Linux Client Crashes with Axis Camera When Dewarping

Title Linux Client Crashes with Axis Camera When Dewarping Description Trying to dewarp an Axis camera on a C-series with the Linux Client on a Server or Linux Workstation using the ExacqVision Client software causes the ExacqVision Client to crash. Product Steps to Reproduce Expected Results Actual Results Solution This works as expected on Windows… Continue reading Linux Client Crashes with Axis Camera When Dewarping

Bad Memory Causes exacqVision Client Crash and System Reboot

On certain exacqVision A Series and Z Series systems, faulty memory causes the system to restart and causes the Windows exacqVision Client to crash (if VGA Acceleration Mode enabled). The following procedure can determine whether the affected memory is installed on a system: <br> WINDOWS Log in to Windows as an administrator.Select the Start menu… Continue reading Bad Memory Causes exacqVision Client Crash and System Reboot