Description:- The client Software crashes once trying to create an even link for the security integration, especially when selecting the DSC security integration alarm input. Solution:- This issue has been fixed on ExacqVision Client Ver23.03.106 and above ExacqVision Client version 23.03.106 can be downloaded Here
Tag: Client Crash
Client restart due to Intel drivers
There is an issue with Intel drivers on Linux systems where customers might call in regarding the client closing or restarting with any of our Linux hardware, but most likely with LC and G-Series PoE is where we’ve seen it. The issue is documented in #d19225. You can tell that this issue is happening because you… Continue reading Client restart due to Intel drivers