Client cannot connect to edvrserver on Windows XP after upgrading edvrserver

Description Client cannot connect to edvrserver on Windows XP after upgrading edvrserver. <br> Introduced Version exacqVision Server 7.7.26+ <br> Fixed Version Not yet fixed <br> Workaround Downgrade edvrserver to a previous version (7.6.x) Since the remote update is not possible, the user has to run an installer on the server manually.