Exacq Unit Crashes When Backup is Imported

Description  When importing a backup file to a NVR the system crashes the machine rendering it inaccessible. After a re-installation the import of the backup file once again crashes the system.  Product  exacqVision Server Steps to Reproduce  Import backup file to the Exacq Server. Expected Results  Settings are imported and exacqVision Server continues normal operation … Continue reading Exacq Unit Crashes When Backup is Imported

Running Windows Chkdsk Command

Title Running Windows Chkdsk Command Description  Chkdsk, also known as Microsoft Check Disk, is a utility that can be used in almost all Windows versions. The Chkdsk commands used to scan through entire hard drives to find and fix any errors. Chkdsk should be run whenever file system corruption is suspected whether by odd behavior… Continue reading Running Windows Chkdsk Command

exacqVision Input/Output, Media, or Write Errors

Description  Meaning of Input/Output Errors, Media Errors, or Write Errors seen in Storage or exacqVision logs. Product  exacqVision Server Information These messages are normally due to a corrupted filesystem or bad blocks on the disk(s). Solution Run ‘chkdsk’ or ‘fsck’. If problem returns, replace the drive. <br>

exacqVision Bad Superblock Message

Description  Meaning Bad Superblock message in logs Product  exacqVision Server Information A superblock is a block of data written at the beginning of a partition that contains metadata about the filesystem. If this block becomes corrupted, a ‘Bad Superblock’ message results.  Solution There are several backups of this data throughout the hard drive and it… Continue reading exacqVision Bad Superblock Message

ExacqVision CRC Errors

Title ExacqVision CRC Errors Description  Meaning of CRC Errors noted from ExacqVision Product  ExacqVision Server Information When data is transmitted from one place to another, checksum value is created to ensure the data has not been altered during the process of being sent. If a discrepancy exists, a CRC Error results.This could result from bad… Continue reading ExacqVision CRC Errors