When installing exacqVision Edge server for Axis cameras, the installation can fail because of an invalid filename, even if the package file exists and the file itself is valid. Because Axis cameras use the Linux operating system, they do not recognize spaces and certain special characters. This can be a problem when Windows appends (1),… Continue reading exacqVision Edge: Axis Filename Cannot Have Space or Special Characters (“Valid Package” Error)