This document assumes you have installed Enterprise Manager version 24.12 or higher and wish to enable SSL for HTTPS connections to the Enterprise Manager webpage. NOTE: For a trusted certificate, it is recommended that you purchase a third-party intermediate certificate from one of many online providers. Exacq cannot guarantee the legitimacy or security of a… Continue reading Enabling HTTPS connections for Enterprise Manager version 24.12. and higherÂ
Tag: Certificate
Creating a Self-Signed SSL Certificate
Before Beginning… Requirements You will need the OpenSSL program to create a self-signed certificate. The method of obtaining this program varies based on the operating system used. Note: A certificate generated on either platform will work on the other (i.e.- a certificate generated using openssl on Linux can be used with a Windows web service).… Continue reading Creating a Self-Signed SSL Certificate
Installer Not Signed or The Signature is Corrupt or Invalid
Description If the DigiCert Trusted Root G4 Certificate is missing, exacqVision Software updates downloaded from exacq.com or initiated within exacqVision Client, will report a signature error. Products Steps to Reproduce Expected Results Actual Results Solution
Enabling HTTPS For exacqVision Enterprise Manager Versions 22.06 thru 24.09
For Instructions on exacqVision Enterprise Manager version 22.03 or older see Knowledge Base Article #12724 The following document details how to enable HTTPS connections to exacqVision Enterprise System Manager from update 22.06 thru 24.09.2.1. For a trusted certificate, it is recommended that you purchase a third-party intermediate certificate from one of many online providers. If… Continue reading Enabling HTTPS For exacqVision Enterprise Manager Versions 22.06 thru 24.09
Enabling HTTPS For exacqVision Enterprise Manager Versions 22.03 or Lower
IMPORTANT For Instructions on current versions of exacqVision Enterprise Manager versions 22.06 or higher see Knowledge Base Article #12804 This document details how to enable HTTPS connections to exacqVision Enterprise System Manager on versions 22.03 or lower. For a trusted certificate, it is recommended that you purchase a third-party intermediate certificate from one of many… Continue reading Enabling HTTPS For exacqVision Enterprise Manager Versions 22.03 or Lower
ESM May Not Connect to Web Service with Self-Signed Certificate
Symptom: The camera video feed section in ESM displays an SSL error message. <br> Problem: ESM may not connect to the exacqVision Web Service if the web service is using a self-signed certificate. This may be more prevalent on systems where TLS/SSL was configured after being added to ESM. ESM did not automatically detect the… Continue reading ESM May Not Connect to Web Service with Self-Signed Certificate
Configuring HTTPS for ExacqVision Web Service
Version 8.4 and Higher Using the provided Web Service configuration UI you are able to configure HTTPS support. <br> Configuring HTTPS using an External Certificate IMPORTANT: Wildcard certificates cannot be uploaded through the exacqVision Web Service administration interface. However, they may be used when manually configured. See Manually Configuring HTTPS for Web Service Certificate and… Continue reading Configuring HTTPS for ExacqVision Web Service