Video Loss on Live View TDVR Capture Card

Description  Reports of 23.09.9.0 Server would cause the Capture Card to show video loss on live page. This was not affecting video recording as live and recorded video were searchable. Product  Steps to Reproduce  Update server from server version prior to 23.09.9.0 Expected Results  Should not show video loss. Actual Results  Live view would show… Continue reading Video Loss on Live View TDVR Capture Card

TDVR8016E Output stops showing Video

Description Server connected to a monitor via output form the Capture Card stops showing video on the monitor when updating to 23.09. Product Exacq Server 23.09 Steps to Reproduce Output works on Server 23.06Update to 23.09 and the Capture Card output stops showing any video on any spot monitors. Expected Results This should work. Actual… Continue reading TDVR8016E Output stops showing Video

How to Re-order Capture Boards with exacqVision

Purpose: After upgrading the operating system or re-imaging an exacqVision server, the capture board order might be changed. In most cases, the board designated Device 2 is now Device 1, and Device 1 is now Device 2. The following procedure explains how to change the capture board order back to the desired order. <br> Step 1:… Continue reading How to Re-order Capture Boards with exacqVision

Assigning the Device Number to an eDVR Board in Linux

To assign the device number to an eDVR board in Linux, complete the following steps.<br> NOTE: This process is usually required when replacing or adding boards. This is the same as using Control Center in Windows. Exit the ExacqVision software.Open the Terminal from Start>Accessories>Terminal.Type the following to stop the Exacq Service: sudo /etc/init.d/edvrserver stopType the following: sudo… Continue reading Assigning the Device Number to an eDVR Board in Linux