How to Re-order Capture Boards with exacqVision

Purpose: After upgrading the operating system or re-imaging an exacqVision server, the capture board order might be changed. In most cases, the board designated Device 2 is now Device 1, and Device 1 is now Device 2. The following procedure explains how to change the capture board order back to the desired order. <br> Step 1:… Continue reading How to Re-order Capture Boards with exacqVision

Replacing an eDVR Board on a Windows-based exacqVision System (Legacy)

The following procedures describe the process for replacing an eDVR board in a Windows-based exacqVision server. If you have an exacqVision server with multiple eDVR boards, complete both procedures; on a single-board system, you can skip directly to the second procedure. NOTE: You must be logged in to Windows as an Adminsitrator to perform these… Continue reading Replacing an eDVR Board on a Windows-based exacqVision System (Legacy)

Assigning the Device Number to an eDVR Board in Linux

To assign the device number to an eDVR board in Linux, complete the following steps.<br> NOTE: This process is usually required when replacing or adding boards. This is the same as using Control Center in Windows. Exit the ExacqVision software.Open the Terminal from Start>Accessories>Terminal.Type the following to stop the Exacq Service: sudo /etc/init.d/edvrserver stopType the following: sudo… Continue reading Assigning the Device Number to an eDVR Board in Linux