The alarm is being generated by the USB DIO module attached to the system. To remove: Windows If logged in as the OS user, close the exacqVision Client by pressing Alt+F4.Log out of the user and into admin by selecting Start > Log Out > select admin > type admin256 > press Enter. Note: admin256 is default. If this… Continue reading Cannot clear a “Power Supply” alarm with USB DIO module attached