ONVIF Cameras May Stop Recording Motion

Issue  Some ONVIF cameras report motion by means of a “pull-point” connection separate from the streaming video connection. If the camera unexpectedly closes the motion status connection, the server will retry the connection in order to reacquire motion status. When this happens, the corresponding server log messages will resemble:4/27/2020 02:59:38.464 AM     onvifnvcPI     Error     http://172.19.232.75:80/onvif/subscribe_service: pull point socket exception.4/27/2020… Continue reading ONVIF Cameras May Stop Recording Motion