Categories
Knowledge Support Support Categories Products exacqVision Integrations

Dahua/Illustra Essentials plugin failed to post NTP server address on the camera at startup.

Description

Dahua plugin which also supports Illustra Essentials failed to set the NTP server on the camera during initial connection time. By default if there is no override ntp server, the plugin should push the address of the server as NTP on the camera.

<br>

Version Introduced

r71495 (dev build 6.5.38.71503/RC build 6.6.0.71575)

<br>

Platform

All

<br>

Steps to reproduce

Factory default a Dahua/Illustra Essentials camera.

connect the camera to a server.

<br>

Expected result

NTP server on the camera should show either the server or override ntp server.

<br>

Actual result

NTP server on the camera stay with the defaulted ntp server(clock.isc.org)

When connect to UNA or Dynacolor Edge, the time could be off as well.

<br>

Work Around

manually override ntp server from client.

<br>

Version Fixed

r103423 (dev build 8.1.8.103450)

<br>

Keywords

Dahua