Description The Camera Recording Page in the client doesn’t show any of the default options such as, IP Address, Camera Name, Video Detection, Record Status, Last Motion, Mac Address, Type, Model, Firmware. Product Exacq Client 23.06 and as early as 22.12 Steps to Reproduce Remove Exacq Vision Client completely from the Recorder, or any client… Continue reading Camera Recording Page Columns Missing on Fresh Install
Tag: Camera Recording
Camera Recording
The Camera Recording page with the ExacqVision Client can quickly provide a high-level overview of the status of all your system cameras from a single page. Use the page to easily compare important camera settings, such as frame rate, resolution, firmware versions, and connection status. You may also apply several settings changes to multiple cameras… Continue reading Camera Recording