Override to Prevent UTC Time Zone Configuration of Vivotek Cameras by the Server

Issue: Adding a camera, disabling or re-enabling the camera, power cycling the camera, restarting the exacqVision server service, or rebooting the exacqVision Server, causes the server to set the camera’s time zone, for all cameras that allow it, to Coordinated Universal Time (also known as Universal Time Coordinated, UTC, UTC+0, UTC+00:00, “Z time”, or “Zulu… Continue reading Override to Prevent UTC Time Zone Configuration of Vivotek Cameras by the Server

New override for Dahua based OEM IP Cameras for UTC Timezone.

Issue: Adding a camera, disabling or re-enabling the camera, restarting the exacqVision server service, or rebooting the exacqVision Server, causes the server to set the camera’s timezone, for all cameras that allow it, to Coordinated Universal Time (also known as Universal Time Coordinated, UTC, UTC+0, UTC+00:00, “Z time”, or “Zulu Time”).  This is preferred for… Continue reading New override for Dahua based OEM IP Cameras for UTC Timezone.