IP Camera Detection Fails If Using Multiple Addresses on Same Interface

Symptom: IP camera detection fails. <br> Problem: If more than one IP address has been assigned to the same network interface on a Windows system exacqVision Server may fail to use correct IP address, thus camera detection fails. Linux is not known to be affected. <br> Solution: Option 1: Temporarily remove all but one IP… Continue reading IP Camera Detection Fails If Using Multiple Addresses on Same Interface