Issue
Starting with exacqVision Server 9.3.21, some ONVIF cameras may repeatedly disconnect and reconnect, which causes gaps in video recording. The following log message repeating pattern may also be observed:
27/02/2020 00:00:27 onvifnvcPI Verbose 172.28.140.17: Context 017 HQ Office R&D. Media open but data timed out. Close and retry
27/02/2020 00:00:27 onvifnvcPI Verbose 172.28.140.17: 017 HQ Office R&D Context 0 Connection status changed to 0
27/02/2020 00:00:27 onvifnvcPI Warning 172.28.140.17: Context 017 HQ Office R&D. Stream closing
27/02/2020 00:00:27 onvifnvcPI Verbose 172.28.140.17: Context 017 HQ Office R&D. Ok to begin playback
27/02/2020 00:00:27 onvifnvcPI Verbose Opening 017 HQ Office R&D. RTSP Uri path: rtsp://172.28.140.17:554/main
27/02/2020 00:00:37 onvifnvcPI Verbose 172.28.140.17: Context 017 HQ Office R&D. Media open but data timed out. Close and retry
27/02/2020 00:00:37 onvifnvcPI Warning 172.28.140.17: Context 017 HQ Office R&D. Stream closing
This issue was introduced when the RTSP streaming implementation was changed in the ONVIF plugin.
<br>
Workaround
Downgrade to latest 9.2.x version or upgrade to exacqVision Server 20.03.6 (and dev build 20.03.110)
Resolution
Fixed with exacqVision Server 20.03.6 (and dev build 20.03.110)
<br>
Version Affected
Starting with exacqVision Server 9.3.21
<br>
Version Fixed
exacqVision Server 20.03.6 (and dev build 20.03.110).