Description If multiple servers share the same IP but have different ports. ESM will remove additional servers with same IP, only using one of the servers. It should include all of these servers. <br> Tested version 4.9.23 <br> Platform All <br> Steps to reproduce Add multiple servers on ESM with same IP Address and different… Continue reading ESM needs to use port and address when building xdv for client