Description As soon as you enable (check the Bosh integration profile . the system will reboot the exacq server service. Product Server Version 20.03 up to 22.12 were experiencing this crash. Panel in use: Bosch B9512GT Steps to Reproduce Configure the Add Security Integrations Page in the Client Select the Enable buttonThe server would lock… Continue reading Bosch Security Integration Causing Operating System to Crash
Tag: Bosch
Bosch Analytics on Newer FW
Description On newer versions of Bosch FW analytics will not work on Exacq. Bosch FW 7.61 is the latest confirmed working version. Steps to Reproduce Configure analytics on Bosch camera.Add camera to exacq server.Setup analytics event linking. Expected Results Analytics are seen and are able to be setup in event linking Actual Results No analytics… Continue reading Bosch Analytics on Newer FW
Bosch (Intrusion Alarm System)
Motion Frames Out of Order on Bosch Cameras
If you see motion images from a Bosch camera that appear to be out of order, the issue can often be resolved by selecting a different setting for the camera’s GOP Structure. To change the setting, complete the following steps: <br> Open the camera’s web configuration page by entering it’s IP address in an Internet… Continue reading Motion Frames Out of Order on Bosch Cameras
Pixelated Video on Bosch ONVIF Cameras
If live video from a Bosch ONVIF camera displays pixelization in exacqVision Client, complete the following steps: Browse to the camera’s advanced mode Encoder Profile page.Ensure that IP is selected in the GOP Structure drop-down list.Ensure that the I-frame Distance slider is configured for a low number (10, for example).Ensure that I-frame Quality and P-frame… Continue reading Pixelated Video on Bosch ONVIF Cameras