Refine Recovery Boot Loader Splash Screens

Description  Definitions for exacqVision Server Recovery splash screens for systems using the refine boot loader. Product  Solution Exacq systems have migrated to a new boot manager called refine.  This new manager has a new look with the same and more functionality than the previous grub boot manager. The new splash screen is icon driven and… Continue reading Refine Recovery Boot Loader Splash Screens

Servers imaged with OPS-21.06.1 Key or reimaged with RETAIL10-21.06.1 Key Break the boot manager after an “apt upgrade”

Issue: Linux servers originally imaged with the manufacturing OPS-21.06.1 Key (which introduced 20.04 OS) or reimaged with the RETAIL10-21.06.1 Key break the “rEFInd” boot manager after running ‘apt upgrade’. Root Cause: The fundamental issue is that the apt upgrade is updating the grub bootloader and overwriting the “rEFInd” boot manager with a new default (“fallback”)… Continue reading Servers imaged with OPS-21.06.1 Key or reimaged with RETAIL10-21.06.1 Key Break the boot manager after an “apt upgrade”