Skip to content

Exacq

Support Portal CMS

Tag: Boards Compatible

Are eDVR boards compatible with an LGA 1156 motherboard?

Yes. Exacq has tested compatibility with the following configuration: <br> *Intel Q57TM Micro-ATX motherboard *Two eDVR boards *PCIe 1x Riser <br> At this time, Q57 is the only chipset that is supported for use with the PCIe 1x riser card. <br>

Published August 30, 2010
Categorized as Knowledge Support, Support, Categories, exacqVision Hardware, Products Tagged Guest, KB-00561-561-210212, eDVR, LGA, Boards Compatible, 1156, 3057

Recent Posts

  • Windows 7 Remote Connections
  • Associations Not Allowed to be saved as Momentary or Sustained Option
  • AVCostar (Arecont) AV20576RS camera model fails to decode H265 in ExacqVision
  • Illustra Edge Analytics
  • Hanwha Edge Analytics
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
  • Remote Connection