A-Series Desktop unit with Motherboard H110E1 is rebooting and stuck on the BIOS password page

Issue:- A-series Desktop unit is rebooting and stuck on the BIOS password page, And when checking in the BIOS, the system drive will be missing and needs to reboot to boot up to windows. Resolution:- There is an issue confirmed by the manufacturer that the new sound card that has been added to the A-Series… Continue reading A-Series Desktop unit with Motherboard H110E1 is rebooting and stuck on the BIOS password page

Updating the BIOS on Systems with ASRock C236M WS Motherboards

Description  The following instructions can be used to update the BIOS on systems with ASRock C326M motherboards. Product  Asrock C236M WS Motherboard Instructions Download the C236MWS3.12E flash file HEREFormat a 32MB or larger USB key as FAT32Copy the flash file to the root of the USB keyPlug the USB key into the NVR and restart… Continue reading Updating the BIOS on Systems with ASRock C236M WS Motherboards

Enabling both HDMI and VGA via the BIOS

Description  How to configure an ASRock system board if HDMI Output has been lost and both HDMI & VGA monitors are being used.   Product  Steps to Reproduce  Expected Results Both monitors display video  Actual Results Video is lost on both monitors  Solution