How to Disable/Enable exacqVision Watchdog Timer

Description  Built by Exacq “BBE” NVRs utilize a watchdog timer, which during normal operation is reset every second. If the watchdog timer has not been reset within 60 seconds it will trigger a system reboot. The assumption being that machine is in a bad state. For various troubleshooting reasons you may need to disable/enable the… Continue reading How to Disable/Enable exacqVision Watchdog Timer

exacqVision Hard Drive Tests

Description  A summary of system drive tests performed by exacqVision using evSelfTest, RAID controllers, and S.M.A.R.T. data. Product  Information On systems Built-by-Exacq (BBE), the exacqVision software runs the following tests: Using evSelfTest.exe: RAID card consistency check, once every week.On non-BBE systems: