Description In order to accommodate more than 4 channels of video, many multi-channel encoders require the use of the “bank” IP plugin override. The cameras test records should indicate this in the Notes. Solution For Example, assuming the cameras IP address is 192.168.1.1: 1st bank would be:192.168.1.12nd bank would be:192.168.1.1#bank=23rd bank would be:192.168.1.1#bank=34th bank would be:192.168.1.1#bank=4… Continue reading Adding Multi-Channel Encoders