Axis Cameras using HTTPS With a Hostname

Description  Axis Cameras running Firmware 9.0 and above fail to connect and stream video when configured to use a hostname instead of IP address and the protocol in the exacqVision Client has been set to HTTPS Required. Product  Steps to Reproduce  In the exacqVision Client: Go to Add IP Cameras. In the Hostname/IP Address field,… Continue reading Axis Cameras using HTTPS With a Hostname

Axis HTTPS setup

To setup an Axis camera for HTTPS support in 8.4.1 server. Log into the camera web page and go to the setup page.Select “System options” and HTTPS.The HTTPS settings page might look different between fw’s.To create self signed certificates, select the create option and fill in the required fields such as country/locality/state/organization/etc in the popup.To… Continue reading Axis HTTPS setup