Archiving

Archiving allows you to create a copy of selected data on another storage device, whether it be an exacqVision S-series storage server, a user provided storage server, exacqVision Cloud Drive, an Amazon S3 account, or Wasabi S3 account. This video explains how to create a new archiving profile, establish the archiving task, then schedule the… Continue reading Archiving

Web service rendered unresponsive if push notifications cannot reach AWS

Affected platforms Web Service 7.2.0, 7.2.1 <br> Symptom In the 7.2.0 release candidate of web service, if the machine the web service is running on does not have access to Amazon Web Services (AWS) for push notifications, the web service will crash on start. In the 7.2.1 release candidate of web service, if the machine… Continue reading Web service rendered unresponsive if push notifications cannot reach AWS

Exacq Software can’t connect to standalone S3 solution

when trying to connect to the S3 internal solution via the Exacq archiving page instead of the standard AWS S3 bucket the system couldn’t establish the connection to it. The standalone S3 solutions are not supported via Exacq Software and the only S3 solution that supported till server version 21.03 is the AWS S3 and… Continue reading Exacq Software can’t connect to standalone S3 solution