Avigilon Camera Motion Detection Fails on exacqVision Server 24.12.7.0

Description  When updating Exacq Server to 24.12.7.0 motion events will stop registering in the Camera Setting page under status last motion event. Motion Events are not being recorded. Product  Steps to Reproduce  Expected Results  Actual Results  Solution

Avigilon H4A Multisensor Camera Not Connecting

Description  Avigilon H4A Multi-Sensor Camera s will not connect and are returning an OnvifnvcPI SOAP receive error. Product  Steps to Reproduce  Add an Avigilon H4A Multi-Sensor Camera Expected Results  Camera connects Actual Results  Camera fails to connect and returns the following log entriies SOAP Error 12/12/2022 02:48:38.640 PM (GMT-8:00) onvifnvcPI Error 172.41.100.124: soap receive error… Continue reading Avigilon H4A Multisensor Camera Not Connecting