*** INTERNAL USE *** With the introduction of the new Authentication mode in exacqVision Client and Server 6.8, the temporary admin password no longer works. However, exacqVision Client includes a way to run in Legacy mode, thus enabling the temporary admin password. <br> This procedure should be used only by Exacq Technical Support. Double-click on… Continue reading Enabling Legacy Authentication Mode
Tag: Authentication Mode
Axis V5915 audio-out fails in digest authentication mode.
Description Audio-out does not work with V5915 fw 5.75.1.4 and set to digest or basic or digest authentication mode. This is a misbehave camera fw that server 8.4 does not support properly. Work around is either revert back to 8.2 or set the camera to basic authentication mode until the issue is fixed. <br> Version… Continue reading Axis V5915 audio-out fails in digest authentication mode.