Server crashes on start-up when audit directory cannot be created

Affected Versions exacqVision Server 7.6 and earlier <br> Description The server will crash on start-up if the audit directory does not exist and the server cannot create a valid audit directory. An example of this is when ‘audit’ is a symlink with an invalid target or a file exists with the same name as the… Continue reading Server crashes on start-up when audit directory cannot be created