Storage Hardware Attribute Alarms from 3rd Party HDDs

Servers are reporting Health Warnings in exacqVision Enterprise Manager.  The event details in EM show “This result is based on an Attribute check on Disk /dev/csmi0,2”  Note: the device may vary for example /dev/csmi0,0 instead of csmi0,2 or perhaps both. The corresponding exacqVision Enterprise Manager logs show: It has been determined that these are false… Continue reading Storage Hardware Attribute Alarms from 3rd Party HDDs