Windows Server 2022 Showing Only One Network Card

Description  Some Exacq NVRs built with Microsoft Windows Server 2022 only acknowledge one network interface, rather than two, when being configured out-of-box. <br> Product  Issue has been noted on BBE systems ASRock Industrial IMB-X1313 system boards, listed below. NOTE: Windows Server OS is an optional upgrade for many systems, so this will not apply to… Continue reading Windows Server 2022 Showing Only One Network Card

ASRock Industrial IMB-X1314 System Beep Codes

Beep SequenceDescriptionTroubleshooting1 short constant beepError with RAM refresh1. Check RAM for physical damage.2. Try another stick of RAM.3. BIOS update2 short beepsRAM parity error1. If adding new memory, try removing to see if this fixes issue.2. Check for conflicts in memory types.3. Check power supply for unstable voltages.3 short beepsRAM read/write test failed1. Repair corrupted… Continue reading ASRock Industrial IMB-X1314 System Beep Codes

ASRock Industrial IMB-X1313 System Beep Codes

Beep SequenceDescriptionTroubleshooting1 short constant beepError with RAM refresh1. Check RAM for physical damage.2. Try another stick of RAM.3. BIOS update2 short beepsRAM parity error1. If adding new memory, try removing to see if this fixes issue.2. Check for conflicts in memory types.3. Check power supply for unstable voltages.3 short beepsRAM read/write test failed1. Repair corrupted… Continue reading ASRock Industrial IMB-X1313 System Beep Codes

ASRock H410 System Beep Codes

Beep SequenceDescriptionTroubleshooting1 short constant beepError with RAM refresh1. Check RAM for physical damage.2. Try another stick of RAM.3. BIOS update2 short beepsRAM parity error1. If adding new memory, try removing to see if this fixes issue.2. Check for conflicts in memory types.3. Check power supply for unstable voltages.3 short beepsRAM read/write test failed1. Repair corrupted… Continue reading ASRock H410 System Beep Codes

ASRock C236M WS System Beep Codes

Beep SequenceDescriptionTroubleshooting1 short constant beepError with RAM refresh1. Check RAM for physical damage.2. Try another stick of RAM.3. BIOS update2 short beepsRAM parity error1. If adding new memory, try removing to see if this fixes issue.2. Check for conflicts in memory types.3. Check power supply for unstable voltages.3 short beepsRAM read/write test failed1. Repair corrupted… Continue reading ASRock C236M WS System Beep Codes

ASRock H110-E1 System Beep Codes

Beep SequenceDescriptionTroubleshooting1 short constant beepError with RAM refresh1. Check RAM for physical damage.2. Try another stick of RAM.3. BIOS update2 short beepsRAM parity error1. If adding new memory, try removing to see if this fixes issue.2. Check for conflicts in memory types.3. Check power supply for unstable voltages.3 short beepsRAM read/write test failed1. Repair corrupted… Continue reading ASRock H110-E1 System Beep Codes

Updating the BIOS on Systems with ASRock C236M WS Motherboards

Description  The following instructions can be used to update the BIOS on systems with ASRock C326M motherboards. Product  Asrock C236M WS Motherboard Instructions Download the C236MWS3.12E flash file HEREFormat a 32MB or larger USB key as FAT32Copy the flash file to the root of the USB keyPlug the USB key into the NVR and restart… Continue reading Updating the BIOS on Systems with ASRock C236M WS Motherboards

Enabling both HDMI and VGA via the BIOS

Description  How to configure an ASRock system board if HDMI Output has been lost and both HDMI & VGA monitors are being used.   Product  Steps to Reproduce  Expected Results Both monitors display video  Actual Results Video is lost on both monitors  Solution