Reverting to Apache Solr After Updating to ElasticSearch (Windows and LINUX)

IMPORTANT: It is advised to update to 22.3.0 so the customer have the capability of doing a backup, then proceed with the update to the version which uses elastic search. Prefix: It is not advised to revert back to a version using Apache Solr unless necessary. It is safer to do a fresh install if… Continue reading Reverting to Apache Solr After Updating to ElasticSearch (Windows and LINUX)

Updating Apache and Apache Solr on exacqVision Enterprise Manager – Windows

To mitigate currently known vulnerabilities, the following updates are recommended. Apache to 2.4.51, Apache Solr to 7.5.0 and exacqVision Enterprise Manager (EM) to 21.12.1 or higher. Note: Updates for both Apache and Apache Solr are available as part of the EM install package for version 21.09 and higher.  However, updating to EM versions 21.12 or… Continue reading Updating Apache and Apache Solr on exacqVision Enterprise Manager – Windows

Can not log into EM after updating to 21.03

Customers report that on Windows 10 units updated to 21.03 they experience an issue when they browse to the localhost to log into EM, it fails with an error that shows: This site can’t be reached.Microsoft link found here detailing other issues similar. HERE If you check the services the Apache service will be in… Continue reading Can not log into EM after updating to 21.03

Solr vulnerability – CVE-2017-12629

Enterprise Manager Enterprise Manager (formerly ESM) includes a version of Apache Solr which is vulnerable to attack allowing remote code execution.  Further information can be found here: https://nvd.nist.gov/vuln/detail/CVE-2017-12629 <br> Mitigation: It is recommended that you follow the steps below appropriate for your Operating System. For Windows Note: File paths vary depending on installation, 64-bit or… Continue reading Solr vulnerability – CVE-2017-12629