To mitigate currently known vulnerabilities, the following updates are recommended. Apache to 2.4.51, Apache Solr to 7.5.0 and exacqVision Enterprise Manager (EM) to 21.12.1 or higher. Note: Updates for both Apache and Apache Solr are available as part of the EM install package for version 21.09 and higher. However, updating to EM versions 21.12 or… Continue reading Updating Apache and Apache Solr on exacqVision Enterprise Manager – Windows
Tag: Apache
Update web service for Apache httpoxy vulnerabilities
Description The version of Apache embedded in the web service has been found to expose a security vulnerability, known as “httpoxy” (technical details: CVE-2016-5387). This vulnerability can be avoided by changing the configuration of Apache. <br> Version Introduced 2.3.9 <br> Platform Web Service / All <br> Work Around Open the evApache httpd.conffile for editingWindows: C:\Program Files\exacqVision\WebService\evApache\conf\httpd.confLinux: /etc/evapache/httpd.confFind and change… Continue reading Update web service for Apache httpoxy vulnerabilities
Can not log into EM after updating to 21.03
Customers report that on Windows 10 units updated to 21.03 they experience an issue when they browse to the localhost to log into EM, it fails with an error that shows: This site can’t be reached.Microsoft link found here detailing other issues similar. HERE If you check the services the Apache service will be in… Continue reading Can not log into EM after updating to 21.03
Configuring Nginx or Apache as a Web Service Gateway
Description The 9.0 release of the web service has replaced Apache with an in-house developed web frontend (WFE) for handling API requests. Certain users may wish to configure a gateway web server to enforce custom policies. The following provides users with a reference for configuring either Nginx or Apache as a gateway. Additionally, it describes… Continue reading Configuring Nginx or Apache as a Web Service Gateway
Hiding a Web Server from Internet Searches (Legacy)
NOTE: This document only applies to exacqVision Web Service 2.4.0 to 8.8. Web Service 9.0.0 replaced Apache with proprietary WFE service. If your exacqVision Web Service is connected to the Internet, the server could be located using certain search parameters in a search engine. To hide the server from an Internet search engine, complete the… Continue reading Hiding a Web Server from Internet Searches (Legacy)