Analytic support for the Illustra3 plugin in server version 8.0.x requires firmware 1.2.x and above. <br> There are two analytic engines, face detection and object tracking. For object tracking rules, the firmware does not provide a unique id but are based on name provided by the user when the the rules are created. Because of… Continue reading Illustra3 – Invalid event linking item when analytic rule name is changed on the camera