Categories
Knowledge Support Support exacqVision Server Categories Products

Illustra3 – Invalid event linking item when analytic rule name is changed on the camera

Analytic support for the Illustra3 plugin in server version 8.0.x requires firmware 1.2.x and above.

<br>

There are two analytic engines, face detection and object tracking. For object tracking rules, the firmware does not provide a unique id but are based on name provided by the user when the the rules are created. Because of that the user has to be aware that if the name of the rules are changed after they are already added to our event linking, the event linking item could become invalid and would need to be updated in our client.