HD Analog Cameras are not Natively Supported on exacqVision Hybrid Servers

Title HD Analog Cameras are not Natively Supported on exacqVision Hybrid Servers   Description  exacqVision hybrid servers do not natively support HD analog cameras too include HD-TVI, HD-SDI, HD-CVI and AHD   Product  exacqVision Server   Solution An encoder which supports HD analog will be required to connect an HD analog camera to an exacqVision… Continue reading HD Analog Cameras are not Natively Supported on exacqVision Hybrid Servers

exacqVision SDVR boards with PAL cameras

Sometimes exacqVision SDVR boards do not immediately recognize the PAL format of analog cameras. Images could be displayed in black and white or even with tearing. If your PAL cameras show those issues when using SDVR boards, complete the following steps in Linux: Log out of the restricted user account and log in as an… Continue reading exacqVision SDVR boards with PAL cameras

Connecting an ExacqVision Hybrid System to a Pelco Coaxitron Translator for Analog PTZ Control

ExacqVision Hybrid servers have the ability to integrate with Pelco Coaxitron CXTA 9760 devices. This allows customers with existing Pelco PTZ cameras that are controlled through the coax with the Coaxitron protocol to be controlled using ExacqVision software. The CXTA accepts the Pelco 422 protocol from the ExacqVision server, and it outputs the data over… Continue reading Connecting an ExacqVision Hybrid System to a Pelco Coaxitron Translator for Analog PTZ Control