Description Some Exacq hybrid systems built since 7/23/2024 and running Ubuntu 22.04 have exhibited a freeze of the analog video after running for some period of time. This is likely a result of a false-positive error state in the PCIe ASPM (Active-state Power Management). This can be confirmed using a Terminal with the following command:… Continue reading Analog video freezing on tDVR 8016e capture boards – Linux
Tag: Analog
TDVR8016E Output stops showing Video
Description Server connected to a monitor via output form the Capture Card stops showing video on the monitor when updating to 23.09. Product Exacq Server 23.09 Steps to Reproduce Output works on Server 23.06Update to 23.09 and the Capture Card output stops showing any video on any spot monitors. Expected Results This should work. Actual… Continue reading TDVR8016E Output stops showing Video
What analog PTZ protocols does Exacq support?
Exacq supports the following RS-422 and RS-485 PTZ protocols. With each protocol, you can specify the baud rate, data bits, stop bits, parity, flow control, and maximum line length. ProtocolSupported PTZ PresetsAD-M320096AD-M3200 Multi96AD-MP4896AD-MP48 Multi96AD-RS42296Bosch (OSRD)99GE-ASCII64GE-Impac32HSD-Pelco-D128Panasonic64Pelco-D32Pelco-P32 <br> NOTE: Devices that require the use of other protocols, not listed above, may still be used with supported encoders.… Continue reading What analog PTZ protocols does Exacq support?
Analog Boards Don’t Work after Upgrading Ubuntu
A directory must be created to make after upgrading Ubuntu. Run the following command in the Terminal: <br> sudo make /usr/local/xdvapi/modules <br> Then restart the services. <br>