Trigger Inputs and Alarm Outputs

Dive into understanding how trigger inputs and alarm outputs work. Become familiar with TTL logic and how to configure devices such as switches or buttons, door contacts, or PIR motion sensors as inputs or triggering outputs to activate lights or more based on events or user input. Trigger Input and Output Alarms help you utilize… Continue reading Trigger Inputs and Alarm Outputs

Server May Indicate False HD Temperature Alarms on Systems with LSI RAID

Symptom Client displays temperature alarms on hard drives. These may indicate temperatures near 1° C, or between ~20000-30000° C.  <br> Problem This behavior was seen from the following Western Digital HD models when connected to LSI storage controllers. WD4002FYYZWD8002FRYZWD8003FRYZWD6002FRYZWD80PUZXWD101KRYZWD121KRYZ <br> Solution Update the ExacqVision Server version to 9.3.9 or higher, also back-patched into 9.2 RC.  <br>