How to Add AD/LDAP Security Group to ESM

Step 1: Log into ESM and navigate to the Domain settings page. If you haven’t yet configured this, you will need to add your domain settings. You must have the proper Base DN, Binding DN and credentials for the account you will use to connect to Active Directory/LDAP. If you do not know these, contact… Continue reading How to Add AD/LDAP Security Group to ESM

Troubleshooting Active Directory Error Messages

Error: “Client Side Kerberos Authentication Failed” Cause: The setspn command was not run on all Active Directory Servers, or there is a duplicate SPN. Solution: On the DC, run the setspn command as directed in the appropriate ExacqVision Active Directory setup guide, or run setspn -X to check for duplicates. If a duplicate is found,… Continue reading Troubleshooting Active Directory Error Messages