Title Acti Motion Windows Disappear exacqVision Server 21.12.2.0 and 22.03.1 Windows Disappear exacqVision Server 21.12.2.0 Description After restarting exacqVision Server service Acti motion windows are no longer present, exacqVision Server versions 21.12.xx and 22.03.1 Product exacqVision Server Steps to Reproduce Update to exacqVision Server 22.03.1Verify motion windows are present on the Motion tab… Continue reading Acti Motion Windows Disappear exacqVision Server 21.12.2.0 and 22.03.1
Tag: ACTI Cameras
Connecting to ACTi cameras with HTTPS
To connect to ACTi cameras using HTTPS requires firmware 6.12.34 or higher, or a signed x509 certificate below version 4. HTTPS connections will work with a version 3 x509 certificate. Self-signed certificates for most ACTi firmware is not supported by the embedTLS library used by the server.
Enabling Multistreaming on ACTi Cameras
To enable multistreaming on ACTi IP cameras, you must activate Dual Stream Mode in the camera’s web interface. <br>