Introduction ACTI A426 camera on Server version 24.12.7.0 had motion recording issues, where they would not record while the camera gui would register motion events.Updating the motion mask from the client reverted after saving. Tested Version Server Version: “25.1.6.0”TESTED roll back to 24.06 – motion was still not working. Platform LINUX UBUNTU 18.04.1 LTS Steps… Continue reading Acti A426 motion not working on Exacq 24.12.7.0
Tag: ACTi
Cloudvue Support Camera List
Cloudvue Supported Camera List
IP Plugin Overrides
The standard form for exacqVision camera addresses is as follows: {host}{?parameter_1=value_1}…{?parameter_n=value_n}{#override_1=value_1}…{#override_n=value_n} <br><br> Overrides PluginOptionUsageACTitransport=httpHTTP stream support for legacy platforms and user dataACTitransport=rtspRTSP stream with separate metadata socket for motion/input trigger/video loss/etc.Axiszoom=configBy default zoom only cameras support.Axiszoom=operationForce zoom only operation and controls as part of PTZ and live view.Axisblocksize=offOn by default, but could turn off blocksize… Continue reading IP Plugin Overrides
ACTi Encoder Multistream Connectivity
ACTi encoder connections require port numbers along with IP addresses to connect to multiple streams (where available).The port numbers for each stream on the encoder should increase incrementally starting with 800. For example, if the IP address of an encoder with four analog streams is 192.168.101.25, the following IP and port number combinations must be… Continue reading ACTi Encoder Multistream Connectivity
Why does my PTZ not work completely on the ACTi ACD2100 camera?
First, make sure that your Analog camera is using Pelco-D protocol and that its address is set to 1. <br> Also, in some versions of the exacqVision software, the speed is not correctly sent to the camera when using the Pan and Tilt functions. To fix this, adjust the speed bar under the Pan and… Continue reading Why does my PTZ not work completely on the ACTi ACD2100 camera?